This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM193: AEC Standard

Part Number: LM193
Other Parts Discussed in Thread: LM2903-Q1, LM393,

Tool/software:

Need to know the AEC standard for below part:-

LM193DR

  • This device does not have any AEC qualifications. (As far as I can see, "Automotive" describes only the temperature range, and it's wrong because the range actually is military.)

    The AEC-qualified variant of the LM393 is the LM2903-Q1.

  • Hello Gauri,

    Clemens is correct. The LM2903-Q1 is the AEC-Q100 qualified version of the LM193DR - which is the extended military temp range (-55 to 125C) commercial part.

    Though the LM193 temp range goes down to -55, and the commercial LM2903-Q1 is -40°C, but otherwise identical.