Part Number: TLC2264
Tool/software:
Hello All ,
To address the problem of capacitive oscillations at the TLC2264's output, I have referred to the app note "Capacitive Load Drive Solution using an Isolation Resistor."
In the theory of operation of application note , it is said that the isolation resistor add a zero which in the end gives the phase boost .

How would a series resistor—a non-reactive component—add a zero to the transffer function, is my query here?
transfer function of output low pass filter adds pole ( 1/(Riso+Ro)*Cload*S+1) to the entire open loop bode plot of op amp ?
Looking forward to the clarification.