Part Number: LM2907-N
Tool/software:
Hello,
I'm a little unclear based on the datasheet if the LM2907 is the right part for my application. I'm working on a safety interlock system for a laser and I have to make sure enough coolant is moving through the laser tube to prevent it from overheating. To that end, I have a Hall effect flow sensor outputting a 0-5V square wave with frequency proportional to the rate of flow. I'm hoping to use the LM2907 to generate a voltage that can be compared to a reference voltage representing the minimum required flow rate. Can the LM2907 function with a Vcc of 5V? If I provide an input voltage of 2.5V from a voltage divider to the 14-pin version along with the Hall effect output, will that suffice for the internal comparator stage?