Other Parts Discussed in Thread: INA333,
Tool/software:
Hello all,
So I'm having an issue with a 4-20mA XTR117 chip that is being fed an input from a INA333 instrumentation amplifier. The 333 chip is having it's gain controlled by a bourns potentiometer (model 3224). The issue I'm experiencing is that when I'm trying to adjust the gain at the 333 for a full scale output of 20mA I'm having a hard time getting it to settle. It seems just by touching the adjustment screw on the pot I see the current reading go up by around 20uA or so. If I use a non-conductive tool to adjust the pot I see that the issue goes away and it doesn't jump once the tool is removed from the adjustment screw. So I'm thinking I'm either injecting noise into the inAmp somehow or inadvertently creating a ground loop with the adjustment screw since the ground for the inAmp is referenced to the Iret pin of the XTR117.
So if anyone has any tips/suggestions I'm all ears on what this problem could be. I have been in touch with Bourns and am waiting to hear what they have to say about this but I thought I would post here also.
Thanks