Part Number: TLV341A
Other Parts Discussed in Thread: TLV3201
Tool/software:
Hi, Staff
TLV341AIDBVT
If the input pin of an op amp exceeds -0.3V,
are there any regulations regarding the current to the input pin?
--------------------------------
Absolute Maximum Ratings
Signal input pins Current ±xxmA
--------------------------------
The following was written in the data sheet for a different model, the TLV3201:
”(2)Input pins are diode-clamped to the power-supply rails.
Input signals that can swing more than 0.5V beyond the supply rails must be current limited to 10 mA or less.”
best regards
cafain