This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM2904B-Q1: VCC or VSS status when input signal comes in to input pin and Power line disconnection status.

Part Number: LM2904B-Q1

Tool/software:

Hi Team,

Customer is asking that any voltage value would be measured at VCC and VSS pins when All power lines are disconnected(or off) but input signal comes in over 12V at V+ and under -12V at V- pins. (in normal operating range)?

And those are ok to use without any damage in normal power-on operating condition?

BR.

Lenny Lee.