Part Number: OPA810
Tool/software:
Hello,
I encountered an abnormal (unexpected) behaviour of OPA810 op-amp in a voltage regulator circuit (attached).

This is a quite common single-supply architecture, where the zener ZD1 is powered from the regulated output via R4. The op-amp, by virtue of R1R5 feedback, scales the zener voltage (nominally 6.8V) to the required output (nominally 10.8V).
For a proper startup, a pull-up resistor R2 is essential. On powerup, due to R2 and finite output resistance of the op-amp some voltage would develop on the output. This voltage, being amplified by the rail-to-rail op-amp, will cause the output to rise, consequently rising the input on non-inverting input. This process ramps up until the zener starts clipping.
However, with OPA810, the circuit fails to start up. Somehow, probably due to some parasitic latch-up type process, particularly possibly when the output is pulled up, some current of about 1uA got injected in both inverting and non-inverting inputs of the op-amp, and some clamping structure between the inputs is possibly activated.
As a result, as the equivalent resistance in the feedback (about 200K) is larger than in the zener filter (100K), parasitic voltage on the inverting input (about 130mV, shown in red) exceeds voltage on the non-inverting input (about 90mV). As a result the output of the op-amp is permanently held low, and the op-amp would not unlatch, even when the supply Vs is at nominal 12V.
Further tests (not discussed here) showed that the op-amp unlatches once non-inverting input voltage exceeds about 130mV.
Thus I found a workaround -- reduce impedance in the feedback below the impedance of the zener filter. For example with R1=27K and R5=47K the circuit does start up.
But the whole situation is worrying for those who do not know. Perhaps you can mention of it in the datasheet or fix the bug in future.
Regards, Alex