Part Number: OPA2206
Tool/software:
過電圧保護について知りたいです。
絶対最大定格信号入力ピン電圧は (V+) + 40 と記載されていますが、電源オフ (V+=0) の状態で入力ピンに 12V 信号が印加された場合、この IC は保護されますか?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA2206
Tool/software:
過電圧保護について知りたいです。
絶対最大定格信号入力ピン電圧は (V+) + 40 と記載されていますが、電源オフ (V+=0) の状態で入力ピンに 12V 信号が印加された場合、この IC は保護されますか?
Hi Matsuura-san,
This figure is what Clemens refers to. I interpret the query based on the translation.
Yes, IC's input terminal will be protected even under the non-powered LDO or V+ state, however, the protection circuit must provide ZD1 for the current path, since most LDOs on the market is unable to sink current.
If V+ is able to sink current, then ZD1 is not required per the query (single supply rail case, where V- = GND).

The same is true for the IC's negative input terminal under-voltage protection as well, assume dual supply rails.

If you have other questions, please let us know.
Best,
Raymond