Other Parts Discussed in Thread: PGA309, ISO124, RCV420, XTR115, LM4030
Do you have PSpice models for PGA309, XtR115, RCV420 and ISO124?
If you have them, please send me to my e-mail.
Thanks in advance.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi,
Unfortunately, we do not have PSpice models for the products you have asked about. They tend to fit in the "system on a chip" category for which simulation models for such products are less common when compared to products comprised primarily of mainly operational amplifiers. Digital interface and control lineas decrease the likelihood of a linear device having a simulation model available as well. Much of a model's availability comes down to being able to define and build models that simulate the product behaviors accurately, and converge well and fast.
Regards, Thomas
PA - Linear Applications Engineering
hi,.
Please can you help me get the spice models for,.24LC02B-E/SN, and PGA309AIPWT,.
Also,there seems to be a difficulty while translating LM4030BMF-2.5/NOPB into the saber,.
Can you please provide the model for LM4030 too.
Thanks and Regards.
Vejeu
Hello Vejeu,
The 24LC02B is an EEPROM. I don't know if TI ever produced it, but if we did it hasn't been in some time. Also, there isn't a simulation model available for the PGA309 as I explained in the original E2E response that you tagged on to.
I suggest you post a message regarding the LM4030 to:
Development tools > Webench Design Center > Simulation & Models
That E2E forum addresses simulation model questions. They may be able to assist you with the LM4030.
Regards, Thomas
PA - Linear Applications Engineering