This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA237: INA237 when using an I2C digital isolator

Part Number: INA237
Other Parts Discussed in Thread: TCA9800

Tool/software:

Options required for I2C communication with the  INA237 when using an I2C digital isolator.

Out digital isolators have a logic low of 0.9V output on the I2C lines. This is above the INA237 0.4V maximum for a logic low.

Is there a new equivalent  part to the INA237 available that has the 85V withstand but also with UM1024  Compliant I2C levels?

Present option being looked at is to buffer with TCA9800 or equivalent but we would  prefer not to add more  circuitry just to get round this issue.