Part Number: OPA4187
Tool/software:
What is the maximum dB possible at 10 kHz, Vs=±5V?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Hiroyuki-san,
This is OPA4187's Aol parameters:

According to GBP, if fp = 10kHz (-3dB), the maximum gains (typical) will be approx. 550kHz/10kHz = 55 V/V, which is approx. 34.8dB

If you have additional questions, please let us know.
Best,
Raymond