This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA241A: Connect -3V to GND

Part Number: INA241A

Tool/software:

Hi,

Can -3V be connected to GND pin of INA241A4 as below schematic?

If yes, is NC connected to GND pin or ground?

input range is 0V to 10V.

Thanks.