Part Number: THS4631
Tool/software:
Hi,
I am using the THS4631 in a high-voltage differential measurement probe where I need to measure an analog signal with a frequency up to 50MHz. A 49.9-ohm resistor is connected between the op-amp's output and the BNC connector. A 50-ohm BNC-BNC cable is used to connect to an oscilloscope with an input impedance of 1MΩ/28pF. I notice that a lot of high-frequency noise is coupled to the oscilloscope input due to impedance mismatch. My output needs to be compatible with a 1MΩ oscilloscope. Is there a way to match the impedance by using any additional components at the op-amp output without using 50-ohm terminators at the oscilloscope input?
Best regards,
Rajhu Baddipadige