Part Number: OPA810
Other Parts Discussed in Thread: THS3491
Tool/software:
1. how to use a operational amplifier to create a negative capacitance values with frequency response with 20Mhz
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello,
Could you explain more about your overall system, circuit, and what negative capacitance values you want to design with an op-amp?
Best,
Alec
Hello Chow,
Can you share your desired amplifier gain, supply voltage configuration, and what the load is for the amplifier?
Best,
Alec
Easy.

Equivalent negative capacitance at the terminals of this thing is -Ceq = C * (R2/R1).
However, GBW of this op-amp shall be well above (your frequency range) * ((R2+R1)/R1). For example, if R2=R1, and your range is 20MHz, I would be using an op-amp with 100MHz GBW, at least 50MHz. Another problem is that, for reliable operation when connected to any circuit, C shall be limited to the maximum capacity, which that op-amp is specified to be able to drive. The higher GBW of the op-amp, the smaller (usually) this Cmax is. R1 and R2 shall be relatively small, so that they do not detrimentally affect stability.
So, all in all, do not expect you can create a "huge" negative capacitance, but about --100pF is not that difficult. Of course it is easier if you need to compensate only a small positive capacitance with that emulated negative one.
And, of course, this op-amp amplifies the signal on its input terminals by (R2+R1)/R1 times, so input signal amplitude shall be limited so that the op-amp does is not clipping. And, needless to say, the same applies to the slew rate -- the op-amp shall not be slew rate crippled at your maximum (20MHz) frequency and maximum expected input amplitude.
I have no idea. I do not work for TI, and suggest you just Google op-amp selection trees from TI and Analog Devices. Usually it is not easy to get +/-15V very high speed op-amps. Most of them are 5V, +/-5V. ADEL2020 is a bit short by bandwidth.
Hello,
The THS3491 meets the slew rate and supply rail requirements of your design.
Best,
Alec