Part Number: OPA551
Tool/software:
Dears,
Can Flag PIN of OPA551 be NC?
Many thanks!
Best Regards,
Arabella Zhang
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: OPA551
Tool/software:
Dears,
Can Flag PIN of OPA551 be NC?
Many thanks!
Best Regards,
Arabella Zhang
Hi Arabella,
Can Flag PIN of OPA551 be NC?
The customer can leave the Shutdown Flag pin open, if it not used. Figure 27 indicates that the pin driving a resistor is optional.
Normally, a current source should connect to some load (e.g. resistor).

The following is OPA551's current specification. If the customer's application consumes up to ±250mA, then they can use OPA593, which is a 4mmx4mm small package and is able operate up to 85Vdc in a single supply or 42.5V in dual rails. We have OPA596, which is the same family as OPA593, but lower in cost (also lower source/sink current up to ±30mA).

If you have additional questions, please let me know.
Best,
Raymond