This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hi Team,
What's the MUX-Friendly function meaning? Could you please help me further understand the benefits of this function? Thanks in advance.
BRs,
Francis
This is explained in MUX-Friendly, Precision Operational Amplifiers.
Most bipolar input transistor and high voltage CMOS op amps require back-to-back input protection diodes to prevent damage when the input terminals are pulled far apart. This fact, however, may cause a long-setting time when one of the diode gets turned-on disturbing input signal. Thus, the need for MUX-friendly input stage that eliminates the need for these input protection diodes - see below.