Part Number: OPA357
Tool/software:
I need an op-amp for an application where I need to quickly enable and disable the op amp. I'm hoping for something like the OPA357, but preferably slower. Does TI have any other parts that meets these specs?
- Enable/disable/shutdown pin with <1us response time
- High impedance output disabled state
- Can tolerate large input mismatch during disabled state (One input driven, one input at VSS)
- Can operate from a single 5V or 6V supply. (15V would probably be OK too)
- Unity Gain Stable
- Gain-Bandwidth >10MHz, <250MHz
- Rail-to-rail in/out preferred
Best regards,
John