This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1211-Q1: Using OUTP only

Part Number: AMC1211-Q1


Tool/software:

Hello team,

To reduce the BOM, are we able to open the OUTN pin as shown below?

In this case, is below correct?

IN voltage = 0V --> OUTP voltage = 1.44V typ
IN voltage =0.5V --> OUTP voltage = 1.44V0.25V=1.69V

Regards,

Hirata