Part Number: INA849
Other Parts Discussed in Thread: TINA-TI
Tool/software:
Hello,
I am trying to determine an accurate value for the 0.1Hz-10Hz current noise on INA849.
On Page6 of its datasheet this is quoted at 100pApp. However, in Figure 7-28 it looks more like 25pApp - a factor of ~4 less.
As another comparison, looking at the datasheet of AD8421 the equivalent figure (Fig 44) shows that amplifier has an input current noise of very close to 1/4 that of INA849 across the relevant frequencies - and the AD8421 has an 18pApp spec and this looks consistent with the time trace in Fig 45 of that datasheet. In other word, all three measurements on the AD8421 datasheet seem consistent with one another and consistently 4x smaller than the INA849 datasheet values (except Figure 7-28)
Taking this information together - and assuming the calculations and characterisation experiments of both devices are broadly similar - it seems the most likely error is in Fig 7-28 of the INA849 datasheet and in fact this data should be scaled (amplified) by approximately a factor of 4 so that it matches the 100pApp spec in the table. If that were the case all three entries in the INA849 datasheet would then be approximately 4x larger than the corresponding entries in the AD8421 datasheet, and would be consistent with one another.
I should note this is an important question for me as I am trying to decide between INA849 and AD8421 for an application in which I want to minimise noise in 0.1Hz to 100Hz range when amplifying a 1k resistance bridge (strain gauge) with 8V across it by a gain factor of 100 to 200.
Thank you in advance for any advice on either clarifying the datasheet or indeed better amplifier choices for my case.