This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

OPA547EVM: jumper settings for non-inverting config

Part Number: OPA547EVM


Tool/software:

I'm not a EE and I'm a little unsure how to interpret table 4 in the user manual. If possible, I would appreciate a photo, or Figure 2 marked up to clearly indicate the physical jumper positions that correspond to Table 4. I took my best shot at it and did not see a waveform on the scope that matched the input from an AWG (arbitrary waveform generator)..

My use case is this: 

  • I’m using the amplifier to drive a voice coil flexure linear actuator (inductive load)
  • Static travel constant for actuator is.27A/mm about neutral mechanical position
  • I chose the OPA547EVM because the manufacturer used the amplifier in a demo and recommended it 
  • Input to amplifier: AWG, 50 ohm output, triangular waveform,  frequency set to 0.5 Hz.
  • When connected directly to actuator +/- 10V (20 p-p) drives the device about +/- .6 mm. So less than 200 mA peak
  • I started with the amplifier output connected to a scope. AWG connected to J5 input. Scope input set to high impedance.
  • Started at low p-p V on the AWG and stopped at around 3 V p-p due to incorrect waveform on scope.
  • Power supply to OPA is 2 channel configured bipolar and set to +/- 10V DC, I buzzed it out (read on a forum that this may need to be increased).
  • The PS can provide +/- 30V DC at 1.5 A
  • I ordered an OVA548EVM to provide more current to drive the actuator to +/- 2 mm, The 547 is on the hairy edge (I think).

I suspect either a jumper is not correct or the supply voltage is too low (or both).

Daniel