Other Parts Discussed in Thread: TPS65131,
Tool/software:
Hi,
I intend to amplify a signal using THS3095DDA. I am using the same circuit as the evaluation board of THS3095 (THS3095EVM Evaluation board | TI.com):
except without any capacitors present on the evaluation board.
I use TPS65131EVM-839 Evaluation board | TI.com to generate a +12/-12V dual supply that is the dual power supply for the opamp. The input to this board is 5V.
So EVAL_TPS65131 is the power supply to a THS3095DDA IC mounted on a SOIC14 adapter and placed on a breadboard. Resistors with the same value as in the EVAL_THS3095 are connected to the op-amp in the breadboard. I also have THS3095EVM Evaluation board | TI.com. When I connect these two evaluation boards, everything works fine and I see an amplified square wave as intended.
The problem is when I connect the +12/-12V dual supply to the op-amp on the breadboard. As soon as I enable the op-amp the supply current continuously rises more than 40mA @ +12/-12V supply to the op-amp and the chip starts heating up.
The weird thing is when I connect the op-amp to a single-ended supply i.e. to +12V/0V, there is no problem and the same chip(op-amp) that heated up now also amplifies the signal without any problem. Is there a grounding problem somewhere, what could be the problem such that a single supply works and dual supply does not?
Thank you in advance!!
PS: The thermal pad of the chip is left floated since it cannot be soldered on a SOIC14 adapter pcb