Other Parts Discussed in Thread: INA116
Hello
I'm a radiometric engineer and would like to design a simple, current input, 0-10V output, precision amplifier module using the INA116 IC.
As it can be read from the INA116 datasheet, it is an instrumetation amplifier, but can it be used as a transimpedance amplifier?
I mean: the current input could be connected to the inverting input (with designing all the guarding stuff as well) the feedback resistor would be connected to the inverting input and the output, the non-inverting input and the "REF" pin is grounded, and the gain setting pins (RGs) shorted for the maximum gain.
Do you think this idea can work?
And my other question: could this circuit work with tee feedback to increase the feedback resistor's effectice resistance?
Thank you for your answer in advance.