This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

AMC1350: What is the differences between AMC1351DWVR and AMC1350DWVR

Part Number: AMC1350
Other Parts Discussed in Thread: AMC1351,

Tool/software:

Hi team

Could you tell the differences between AMC1351DWVR and AMC1350DWVR?

It seems that there are diffrences about input voltage range and output voltage range as below. Are there any differences else?

AMC1351

input voltage range : -0.25 ~ +5V

output voltage range : -0.1V ~ +2V 

AMC1350

input voltage range : -5V ~ +5V

output voltage range : -2V ~ +2V 

Regards,

Noriyuki Takahashi

  • Hi Noriyuki,

    Yes, the main differences between these devices should be the input/output ranges. Namely, these differences stem from AMC1351 being a single input device and AMC1350 being a differential input device. Please let me know if there are any more questions. 

    Best regards,

    Eva