Other Parts Discussed in Thread: BUF802,
Tool/software:
I need to drive a 1GHz signal on a 1m 50ohm coax cable and am considering either OPA859 or BUf802. The OPA859 is in unity gain configuration and is somewhat preferable due to lower input capacitance.
- Can both of these amplifiers directly drive a coax cable or is an additional cable driving buffer preferable?
- Is there a need for series termination at the amplifier output? The cable is terminated into 50 Ohms at the far end.
- Is there a reference design with layout for driving a cable with low distortion at about 1GHz?
Thanks a lot