Part Number: TLV9062-Q1
Other Parts Discussed in Thread: LMP7716-Q1, OPA2317-Q1, OPA2377-Q1, LMV772-Q1, OPA2991-Q1
Tool/software:
Hi Team,
I'm promoting the TLV9062-Q1 to my customer to replace the competitor's solution. Could you please help check below questions?
Below is their test condition.
Vs=5V, IN+=IN-=0-130mV, VCM=0-65mV, Vout=0-3.3V, Gain=25.
Vout=1.67V at IN+=65mV, Vout=3.3V at IN+=130mV, Vout=0V at IN+=0mV.
The customer is concerned that there will be a large error in the output at low IN+.
Based on customer's test condition, may I ask if the offset voltage drift (µV/C) can meet the range of 0.4uV to 1.6uV at TA = –40°C to 125°C? May I know if Vos meets the normal distribution of -500uV to 1000uV at their test condition?

Below is customer's original schematic.

Thanks!
Regards,
Ivy