Part Number: AMC3311
Other Parts Discussed in Thread: AMC3301EVM, AMC3301, AMC3330
Tool/software:
Sorry I took to long to investigate so the thread was locked.
To answer your questions:
Could you provide some more information on your system?
What are the 3 AMC3311s being used to measure?
The AMC3311 is used to measure voltages 0 to 300VDC. Very slow voltage change (battery voltage) so the response does not need to be fast.
As seen on the screenshot of the schematic in original thread there is a voltage divider with 1Mohm resistors on each side of a 10kohm resistor. The AMC3311 measure over the 10kohm resistor.
Are you seeing the offset on all the devices?
Yes, but it varies between ICs. I have now desoldered the two left ones and only focused on the position to the right on the PCB. There is no improvement so my idea that they are interfering with each other was not true. I have tried two different ICs and one shows 1,5mV on output and the other shows 9mV on output (when shorted on input before the 1Mohm resistors).
If shorted after the 1Mohm resistors (closer to the AMC3311, same as shorting the 10kohm resistor) then there is very low output voltage (it is then within my offset requirement).
When you say 0V input, does that mean your input supply is off or is the input being forced to 0V?
I mean the ICs are powered, i.e. the PCB is on. But the input is shorted as described above. I have to force the input to 0V using a screw driver or some other way to short the traces. If I do not short the input (but still supply 0V over the resistor divider) then there is 1,5V or 9mV depending on IC on the output which means my product will not show 0V in the LC-display when the battery voltage is 0V.
As mentioned before, the ICs are very temperature sensitive. Putting my finger on the IC makes the output rise several mV.
I have ordered new AMC3311 chip. Also AMC3301 and the AMC3301EVM are on order. I will see if those are better.