Part Number: INA381
Other Parts Discussed in Thread: TLV9152, , LM2903, INA180, TLV3231
Tool/software:
Hi team,
I'm looking for op amps and comparators that enable high-speed overcurrent detection for compressor motor. Could you tell me the fastest solution for this?
[Requirements]
Offset voltage: <1,000 UV
Slew rate: >10 V/us
Package: SOIC (2 in 1)
GBW (MHz): >0.5 MHz
Supply voltage: >4.5 V
Short-circuit protection should be done in us.
TLV9152 + compressor is too slow.
My first thought is INA381. Alert is outputted in about 2.3usec in response to a 0.1V shunt voltage rise. Slew rate is not good enough(2V/us).


And I olso thought INA180 + LM2903.
What is the fastest solution to output alert? I hope you will give me multiple options.
Regards,
Hiromu