Part Number: OPA828
Other Parts Discussed in Thread: TINA-TI
Tool/software:
I have built the circuitry shown below, which is a 1 MHz amplifier capable of driving at 150 ohm load with up to +20 V. When loaded with too high capacitance (a 2 m RG58 coax), modelled with Cload, it starts to oscillate at 12 MHz. When I simulate the circuit in TINA-TI I am not able to reproduce the actual oscillating behavior.
The TINA-TI simulation does not oscillate even if I grossly exagerate component values, which should make the circuit unstable. I therefore suspect there is something wrong with my usage of TINA-TI.
More details:
As I understand to get stable circuit the feed-back pole consisting of R7||R10 * (Cstab+ C_opamp_neg_input) should be = 100 MHz > 2 * GBW / gain = 45 MHz / 5.3 = 8.5 MHz, thus amply fullfilled. Changing Cstab to 100 nF however does not make the circuit unstable. Increasing Cload dramatically also does not make it unstable. Only by using R7 = 1 Mohm & R10 = 4.7 Mohm was I able to get an oscillating output.
Am I doing something wrong with TINA-TI ? Is there an obvious parasitic component that I miss to add (long inductive wires to Q1) ?
The TINA-TI component references match the reference designators in the pcb picture.