Part Number: TL082
Other Parts Discussed in Thread: , OPA2182, TLV9352
Tool/software:
Hello:
For equipment using TL082, when using the signal generator for TL082 of batch 22+, the flow fluctuation is small, and the fluctuation value is generally 1-2mm/s. After replacing the TL082 of batch 23+, the flow fluctuation is large, above 6mm/s. This phenomenon can be reproduced by various models. If the TL082 of batch 23+ is replaced with the TL082 of batch 22+, the abnormal phenomenon will disappear. Please confirm with the original manufacturer whether the TL082 of batch 23+ has a change in process/factory that causes the spec change
The following two photos are good products tested, batch number 2304


The following two photos are bad products tested, batch number 2345


The customer's current inventory and early shipments are all batch 2345. In addition, the silk screen layout of these two batches is completely different. The silk screen of the chips shipped by the customer before the problem was discovered is all similar to batch 2304.
PCN file is attached,please help check