Part Number: PGA855EVM
Other Parts Discussed in Thread: PGA855,
Tool/software:
Hi TI,
I found that when I change the gain setting on the EVM, the bias current also changes.
The PGA855 is powered from +30V and -4V, with VCC = LVDD+, VEE = LVSS-.
Inputs are connected to GND, and outputs are left open. I can measure 12.94V (close to 13V from mid supply internal VCM biasing).
The gain setting is changed by shorting/ opening the jumper on A0, A1 and A2 jumpers.

What I observed is that, with more switch connected, it seems my bias current also increases.
At 000 gain, the positive and negative bias currents are equal.
At 100, the positive bias current increased by 3mA.
Then at 110 or 011, the current increased by another 3mA.
At full 111 gain, the current is now at 3x 3mA increase from 000 gain.
I checked the digital pins settings, but I think I am not overstressing their voltage limit:
There is also pull down resistors at the gain setting jumpers, but with 100kohms, I am not expecting >1mA of increase.
What is this behavior that I am looking at? Should I be concerned?