Part Number: PGA308EVM
Other Parts Discussed in Thread: PGA308,
Tool/software:
I'm attempting to follow the flow chart in Figure 5-14 of the user manual.
I'm using an Arduino Uno to drive & a logic analyzer on vout_F to verify steps.
The register reads & writes seem to be going as expected but the vout doesn't seem to be enabled afterwards.
I have a few questions:
1) does this mode require a power cycle prior to each start?
2) is it required to disable one-wire (CFG2 D15 = 1) after reading / writing to RAM registers?
3) in order to successfully use this mode, do I need to do any of the steps shown in figure 5-14 other than those that mention "Read" or "Write" (e.g. do I need to disable checksum or enable one-wire or disable one-wire timeouts)?
4) will One-wire reads & writes still work in this mode even if I set DIS OUT = 0? If not, at what point on the flowchart is it appropriate to set DIS OUT?
If it helps, here is the output from the logic analyzer:

Regards,
Rob