Part Number: INA233
Tool/software:
hi, I am FAA NCG in Taiwan and I have some questions form the customer side regarding to the application of INA233.
1) Are we able to connect PMBUS directly to BMC so that BMC could read the current voltage/current/power in application?
2) I2C/SMBUS/PMBUS interface's voltage reference is set by the value of the external pullup resistors?
3) Could we use it with a load current around 25A since the load current is 10A In the typical application we provided in TI's data sheet. What is the maximum load current?
Thanks for the help