Other Parts Discussed in Thread: LM2902LV, TLV9002
Tool/software:
I have designed a high amplification circuit to amplify a weak signal from a photodiode. It works well, but it is sensitive to temperature. The temperature range is usually between 18-30°C. Temperature affects the signal level directly. After some testing, I found that temperature affects the feedback resistors, even though they have a low temperature coefficient. I suspect this could be due to the differing thermal properties of the circuit board, solder, and resistors, but I'm not sure. I have built a temperature isolation case for the circuit, which prevents sudden fluctuations, but temperature still affects the signal level. Do you have any advice to correct the problem or suggestions for changes in circuit design to achieve the same gain without temperature sensitivity?