Part Number: INA233
Tool/software:
Hi,
I have been using INA233AIDGST current sensor to read the 5V input voltage and Max 5A load current but i couldn't read any current consumption.
The shunt resistor value which i have used is 0.005E power rating of 0.25W. Is this the correct power rating to read the 5A load current? if not kindly suggest me the respective power rating value to read the Max 5A load current.
I have attached the schematic diagram of the current sensor for your reference. Kindly refer the attachment