Part Number: TLV1822-Q1
Other Parts Discussed in Thread: TLV1822
Tool/software:
I am working with the TLV1822.
supply voltage: 12V
threshold voltage: 2.5V
input voltage: 0V-10V square wave, 100 Hz

I have it setup for a hysteresis of:

Here is what I am seeing:

The middle trace is on the positive input (pin 5 in the schematic above).
I am not sure what's pulling it up so far above ground. I am not a EE so please forgive me if it is something obvious.
Note: the signal looks correct at the filter.
When I simulate it in Tina I do not see this behavior:

Any help is appreciated.