Tool/software:
Hello
I want to monitor current of the load,
INA226 can be measured the below current spec. ?
Required Spec.
1. Current sesnsing Range : 200 uA ~ 500mA
2. DC Power : 12 V
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Tool/software:
Hello
I want to monitor current of the load,
INA226 can be measured the below current spec. ?
Required Spec.
1. Current sesnsing Range : 200 uA ~ 500mA
2. DC Power : 12 V
Thanks.
Hi Jeehoon,
The shunt voltage input range is +/- 81.92mV and the Ib is 10uA. Assuming you're using a shunt resistor of 2mOhms, your current sense range would be within the rated spec and however your minimum current of 200uA is of the same order as the Ib (10uA), so you may see some offset in your readings.
Best,
Mallika Senthil
Hi. Mallika Senthil
you meaned that I can monitor current from 200uA to 500mA (12 V DC on Load device) if I use to test it with INA226 Evaluation Module.
is it riight?
Best regards
Yes you can measure that range of current, but there will be 10uA of offset.
Best,
Mallika Senthil