Tool/software:
I would like to know about the TI op-amp OPA462. I am creating an amplifier circuit using the above product, but I am not able to amplify as I would like. I have created an inverting amplifier circuit with a magnification of about 20x. 80V is applied to V+ and GND is connected to V-. I am expecting 100-5V to be output when 5V is applied to IN+ and 0-5V is applied to IN-, but the actual output range is 24-5V. The output becomes 24V when IN- is around 4V, and it seems to be capped. Since RL is 10kΩ, I thought it would be possible to output up to V+-1.5V (78.5V in this case). What do you think is the reason why it is capped at 24V? *Other terminals are connected as follows. E/D terminal: 5V E/D com: GND Status Flag: N.C