Part Number: INA228
Tool/software:
I am using the SCB controller to talk to the INA228 that I have on my board (via I2C) by wiring the SCL, SDA, 3.3V and GND from the INA228 to the SCB. I use the same GUI as the eval board. I set the address SW0 and SW1 to match the address of my INA228. I try to configure the registers to my desired setting in the GUI. However, when I click "Write All Register", the "MODE" under ADC_Config changed to "SHUTDOWN". I observe no clock signal at the SCL. Can you advise if I can actually use the SCB this way? What could be wrong that cause it to go to SHUTDOWN? Below is my INA228 schematic. Thanks