Customer looking to THS4120 (or THS4130) for a new design. It will take its input from a hydrophone and output to a AD1974 ADC... I have the THS4120 Datasheet... I was wondering if you can point me to a reference design or other that would provide some guidance (or things to watch out for, etc...). I need to use a single power supply ~ probably 3.3VDC, but maybe 5 VDC.
thanks