Part Number: THS2630
Other Parts Discussed in Thread: THS4541
Tool/software:
Hello,
I am planning on using THS2630 for my ADC application circuit. My ADC on the board accepts 2.5Vpp. Input signal to the board is 20Vpp. I am thinking of using THS2630 to convert 20Vpp signal to 2.5Vpp @3MHz just before ADC.
On datasheet of THS2630, I do not see any example of attenuation of input signal. As for TINA simulation, yes it is possible. I just want to make sure.
Also, Spice file for THS2630 is not working at all. Simulation is so slow that it takes 10 mins for 2ns of simulation time. There is only THS2630 on simulation.
Thanks in advance
Alper