Other Parts Discussed in Thread: INA700, INA232, INA238, INA228
Tool/software:
Hello,
I am trying to measure current and power of a voltage rail (~3V) with INA700EVM, the average current level is in between 1 - 6mA. Based on the simulation results given to us, there should be around 1mW or less. Is it possible to use this INA700EVM? If so what would be the best setting for the conversion delay to set up for about 4K-5K samples. I appreciate if you can give us some advise. I also have a INA232EVM and installed a 12mΩ current sense resistor. based on the
Thanks,
William