This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

INA186-Q1: Impedance

Part Number: INA186-Q1

Tool/software:

Hi Expert,

Customer wants to know the input impedance of IN+, IN-, which is not displayed in data sheet. Can you give a support?

what does the impedance consists of?

  • Hi Beida,

    I'm not sure if the customer is enquiring about the input impedance of IN+/- pin to GND or the differential input impedance (Rdiff) that is present within the device as shown in the diagram below.
    Rdiff is typically around 2Mohms or between 4-5 Mohms as shown in the graph below. A1 - A5 being different gain values.

    The impedance of the pin with respect to GND can be calculated as follows:

    R = Common mode voltage / Input bias current = Vcm / Ib = 12/(0.5nA) = 2400 MOhms.

    Since these are devices that are connected to a DC supply, you can consider the impedance to be purely resistive.

    Best,
    Mallika Senthil

  • Hi Mallika,

    Thanks for your update.

    Customer is asking the input impedance of IN+/- pin to VCC, which is found in data sheet. Can you give a support for the impedance value and calculation process?

    The IN+/- input structure to VCC is BJT or CMOS?

  • Hi Beida,

    The calculation would be the same as in my previous post. Take the voltage on the line IN+/- is connected to and the bias current at the input (Ib = 0.5nA), then use Ohms law to calculate the impedance.

    Best,
    Mallika Senthil

  • Hi Mallika,

    I didn't see the electronic path from IN+/- to VCC, so I am confused on your guidance. Why bias current can be used to calculate the input impedance?

    If Vs = 5V, IN+/- = 24V, can you give the calculation process for impedance between IN+/- and VCC?

  • Hi Beida,

    The connection path your referring to is internal to our device and is TI intellectual property. All customer relevant information is specified in the datasheet.

    Best,
    Mallika Senthil