Tool/software:
Dear team,
Do we have a bidirectional current sense amplifier with internal reference?
For example, INA186-Q1 requires an external input reference to achieve bidirectional current sense amplification.
Now my customer wants a Q1 chip with corresponding functions without external REF.
Mainly use it in the SHUNT current sampling part.
The input voltage range is: -50mV~+50mV.
The required gain is 50, and 5V power supply and realize bidirectional current detection (detecting the negative differential voltage and positive differential voltage from both ends of the SHUNT). The internal reference voltage is preferably half of the power supply.
Thanks and I'm looking forward to your reply!