Part Number: ALM2403-Q1
Tool/software:
Dear TI team
The temperature in front of me is ALM2403.
I have a small problem, the imported electricity is 20V, the calculation according to the standard is Vout for 20V/2, RL is 75 ohm, as shown below.

Calculated loss 1.37W.

Use RθJA to calculation the temp is 149C, it is very high temp in IC.
but if i use RθJC(bot) to calculation the temp is 93C

1. Why should I use the individual calculations?
2. Do I have any problem with my calculations?
3. Or is it a calculation that I have in mind?