Part Number: OPA2890
Other Parts Discussed in Thread: OPA890, THS3491, LMH6703
Tool/software:
Dear Technical Support Team,
What is the maximum frequency of the OPA890 for square wave?
10MHz seems to operate correctly, however 250MHz (500Mhz) is required for next version of my application.
output square wave signal is from 0V to 4.5V.
I think general method of calculating the sine wave slew rate is as follows.
SR= 2πfV=2x3.14x250MHz*4.5V=7,065V/us
Q1.
Is the slew rate calculation method for a square wave the same as for a sine wave?
Q2.
Could you suggest appropriate high speed amp for 500MHz(250MHz) square wave?
Best Regards,
ttd