Part Number: AMC1311
Other Parts Discussed in Thread: ISO224
Tool/software:
Dear.Ti
I would like to know what will happen to the states of OUTP and OUTN when Vin(VDD1) is turned off.
If Vin(VDD1) is ON with SHTDN in low state, I wonder if OUTP and OUTN will be output as LOW.
In my opinion, it seems that under such conditions, VCMout(1.44V) or Max Vout may occur.
I want to apply an IC where OUTP and OUTN are set to Low outputs when Vin(VDD1) is off and Vout(VDD2) is on.
please let me know if there's any device available for this purpose.
Best Regard