Other Parts Discussed in Thread: INA128
Tool/software:
I'm trying to run simulations on INA129 and I'm using the model in PSpice for TI, but surprisingly the pin numbers & names in the model don't match the ones in datasheet.
The model has 10 pins and datasheet has 8 pins only. What am I missing?
Below is the comparison of the pin numbers, middle column is from datasheet and third column is from spice model:
Pin 1: RG / VIN+
Pin 2: VIN- / VIN-
Pin 3: VIN+ / V+
Pin 4: V- / V-
Pin 5: REF / VO
Pin 6: VO / -
Pin 7: V+ / -
Pin 8: RG / REF
Pin 9: - / RG
Pin 10: - / RG