Tool/software:
I am using the LMP7704 as a buffer. When I perform an AC Analysis with the op amp supplied with +5V and -5V, the analysis shows a magnitude of 0dB at low frequency, which is what I would expect for a buffer with a gain of 1. If I supply the op amp with a single supply of +5V, the AC analysis shows a magnitude of -44.19dB at low frequency. What would cause the simulation using a single supply to give different results?