Other Parts Discussed in Thread: INA260
Tool/software:
Hi,
We are planning to measure isolated voltage (Vbat) using the INA226 and need some assistance with the circuit design.
- Which ground should be connected to the ground (pin no.7) of the INA226?
- Is Vbus (pin 8) referenced to the INA226 ground (pin no. 7)? If so, would this result in a short between the two grounds in our system?
Note: We have two isolated power supplies: 5.0V (DGND) as VS and Vbat (PGND) as VBus. The 5.0V supply is used for the MCU, while Vbat is used for the power section.

Thank you.
Regards,
Sivam Natesan