Part Number: THS4561
Other Parts Discussed in Thread: THS4551
Tool/software:
Can you please provide some guidance regarding the PCB Layout mentioned on page 36 of the THS4561’s data sheet. I am using the WQFN 10 pin package (the diagram on page 36 only shows the layout for the VSSOP). My question is that the data sheet recommends to cut out the power and ground planes underneath the components as shown on page 36. However, it also recommends that vias be placed close to the supply pins that are located in the cut out area where there is no plane to connect to. I could run a trace, from beyond the cut out section, to the via but that seems counter intuitive to add that extra impedance. The WQFN package seem to be more applicable for less cut out area due to the power pins being located at the two ends of the package. Any advice on this would be appreciated.